REC.TRIGVAL

Description

REC.TRIGVAL is the value that must be met by REC.TRIGPARAM for the trigger to occur. The units of this parameter are set according to the units of REC.TRIGPARAM.

Examples

Code

Sets the value to use as trigger to be 1024. Only when REC.TRIGPARAM matches this value determined by what REC.TRIGTYPE is set to, will the triggering happen.

-->REC.TRIGVAL 1024

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

The units of the parameter are chosen according to the unit type.

Range

-9223372036854775.808 to 9223372036854775.807

Default Value

0

Data Type

Float

See Also

REC.TRIG

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.